AXIS#.FBUS.BLOCKING
Description
The AXIS#.FBUS.BLOCKING command returns the actual protection state if AXIS#.FBUS.PROTECTION is set.
| Value | Description |
|---|---|
| 0 | Commands are not blocked for “service channel” access. |
| 1 | Certain commands are blocked and can not be accessed by “service channel” because the fieldbus master has control. |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.FBUS.BLOCKING |
5005h |
02h |
Unsigned8 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5103 |
1 |
5103 (0x13ef) |
AXIS1.FBUS.BLOCKING |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.FBUS.BLOCKING |
5103 |
Unsigned8 |
Read Only |
- |